Hi,
While going through the HSDC PRO GUI Software manual, I see like based on SYSREF signal's rising edge data capture starts automatically, in
the section 3.1.3.4.4 Read Captured Memory from the Slave Board of the document downloaded from the following link.
http://www.ti.com/lit/pdf/slwu087
But it was added under the section 3.1.3.4 Using Multiple TSW14xxx and ADC EVM’s for Simultaneous Capture using Trigger Option.
My doubt is can we use this SYSREF signal based capturing option for TSW14J56EVM when used as only one board.
If yes what is the procedure?
Please Reply asap.
Thanks,
Ayyappan M.