This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/ADS131E08: setup C code

Part Number: ADS131E08

Tool/software: Code Composer Studio

Hi, 

I require a sample C code for configuring the ADS131E08 in CCS. Could somebody help me? 

Thank you. Best regards, 

Carlos 

  • Carlos,

    I'm going to point you to the following E2E post:

    This should have some firmware that was written with the EVM. I don't do a lot of coding, and I'm not entirely familiar with this example code. However, I hope that it can help you get a good start.

    Note that the link is with the ADS130E08EVM, and note the ADS131E08EVM. This was an error in packaging up the software for the EVM.

    Joseph Wu