This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298ECGFE-PDK: Data not receive on channel

Part Number: ADS1298ECGFE-PDK
Other Parts Discussed in Thread: ADS1298R

Hello,

I am interfacing the ADS1298R Evaluation board with an Cortex M3 MCU.

I am working with TI's default configuration for power i.e +- 2.5V supply .

I have configured and test for internal as well as external clock reference but the result is same .

Following are my logs on serial terminal but the data is always 000 when my ECG simulator is ON .

Please help.

Thank you.

*******************************************************************************************************

18:38:10.818 -> -- ID210-----------------------------------------------------------
18:38:10.852 -> CONFIGs 1 2 3
18:38:11.978 -> ---------------------------------------------------------
18:38:11.978 -> Check Configs
18:38:11.978 -> CONFIG1: 2        0x02
18:38:11.978 -> CONFIG2: 160        0xA0
18:38:12.011 -> CONFIG3: 192        0xC0
18:38:12.011 -> ---------------------------------------------------------
18:38:12.011 -> Set Channels
18:38:12.144 -> ---------------------------------------------------------
18:38:12.144 -> detecting active channels:
18:38:12.144 -> gMAXChan: 8
18:38:12.144 -> 1: 96        0x60
18:38:12.144 -> 2: 96        0x60
18:38:12.144 -> 3: 96        0x60
18:38:12.144 -> 4: 96        0x60
18:38:12.177 -> 5: 96        0x60
18:38:12.177 -> 6: 96        0x60
18:38:12.177 -> 7: 96        0x60
18:38:12.177 -> 8: 96        0x60
18:38:12.177 -> detected 8 active channels.
18:38:12.177 -> Device Type (ID Control Register): 210 Channels: 8
18:38:12.177 -> Inside read_and_send_data 8 active channels.
18:38:12.177 -> -Channel 1
18:38:12.177 -> **************************************
18:38:12.177 -> 0 0 0
18:38:12.177 -> -Channel 2
18:38:12.177 -> **************************************
18:38:12.177 -> 0 0 0
18:38:12.177 -> -Channel 3
18:38:12.177 -> **************************************
18:38:12.177 -> 0 0 0
18:38:12.177 -> -Channel 4
18:38:12.210 -> **************************************
18:38:12.210 -> 0 0 0
18:38:12.210 -> -Channel 5
18:38:12.210 -> **************************************
18:38:12.210 -> 0 0 0
18:38:12.210 -> -Channel 6
18:38:12.210 -> **************************************
18:38:12.210 -> 0 0 0
18:38:12.210 -> -Channel 7
18:38:12.210 -> **************************************
18:38:12.210 -> 0 0 0
18:38:12.210 -> -Channel 8
18:38:12.210 -> **************************************
18:38:12.210 -> 0 0 0