Part Number: ADS1298
Other Parts Discussed in Thread: ADS1198,
Hello.
I have a question about the external reference voltage range of the ADS1198.
The specifications(Recommended Operating Conditions) are as follows.
3V Supply: VREF = 2.5V (NOM)
5V Supply: VREF = 4.V (NOM)
(When 5V Supply(AVDD=+2.5V, AVSS=-2.5V), GAIN = 1)
・ There is no problem in inputting VREF = 2.5V, right?
・ When VREF = 2.5V, the input near VIN = -2.5V or + 2.5V is saturated, does ADC-CODE not reach 8000h and 7FFFh?
(FSR=±2.5V, VIN-Range: -2.2V ~+2.2V)
・ When VREF = 5V is input, does the ADC-CODE with VIN = -2.5V to + 2.5V output only up to about C001h and 3FFFh?
(FSR=±5V, VIN-Range: -2.2V ~+2.2V)