Other Parts Discussed in Thread: ADS1192, , ADS1292R, ADS1291, ADS1292
Folks,
The ADS1191 (single channel) and ADS1192 (dual channel) share the datasheet. I'm looking for the pinout for ADS1191. I've found the drawings on p.9 and the table on p.10 . The table has a single column, which doesn't differentiate between the ADS1191 (single channel) and ADS1192 (dual channel). The table also shows the third pair of differential inputs.
Fig.14 shows RESP_MODP/IN3P and RESP_MODN/IN3N; neither AD1191 nor AD1192 is supposed to have a drive for impedance pneumography.
Which [single in case of ADS1191] channel is are actually connected? To which pins?
Is the second PGA active in ADS1191? If so, how should I treat it?
Is there an accurate document for ADS1191?
Any suggestion, insight or reference is really appreciated!
Cheers,
- Nick
p.s. The present version of the ADS1191 datasheet looks as if somebody took the datasheet for ADS1292R, started removing the bits which don't apply to ADS1191, removed half of them... and didn't finish the job.