Hi all,
Our customers are concerned about:
Q: The thermocouple electromotive force is applied even when the ADC is power off.
Since the electromotive force of Thermocouple is very small, I think that there is no problem if it is within the absolute maximum rating, but is there any countermeasure for TI ADC (eg ADS122C04)?
Even if there is no countermeasure, if it is within +/- 300mV from the ABS MAX specification of the device, I think there is no problem. Is it correct?
Best regards,
Hiroshi