Hi,
I have a problem with the combination of the EVM Motherboard DSP5515 and the FE-Board with the ADS1298.
I use the Code from the following side: http://code.google.com/p/c5505-ezdsp/
After I debug the Code, the display on the board show only the information on the front of the display and not the signal. In addition I can´t connect the PC Applikation.
When I connect the ADS1258-FE and debug the code for this board, everything is ok.
Can everybody help me?
Regards
Heinrich Reimer