Other Parts Discussed in Thread: ADS1232REF, ADS1232
I have purchased the ADS1232REF evaluation board from Digikey and have downloaded the SBAU120A User's Guide dated Sept 2007.
Board is connected to a balanced 120 ohm strain gage bridge with about 1 meter of twisted / shielded lead. Power is from 9 volt dc wall mounted pack. Excitation is 5 volts, board supplied. Board is connected via USB to a desktop PC running XP Pro.
The instructions do not appear to correspond to the switch functions on the board. For example, entry into the configuration mode uses the PARM buttons, not the ENT and SEL buttons as instructed. Calibration proceeds normally until I try to exit back to scale. Most often the numbers shown seem to steadily increase until they hit the max. TARE does not seem to work at all. Values change inadvertently and are not reliable. Using the SBAU120A guide, I am unsure about the procedures to enter, exit, and save the calibration values.
Is there a corrected instruction set that actually corresponds to the configuration of the eval board? Post's re the ADS1232REF do not seem to have these troubles. Is this a unique problem on this particular board?
C