Part Number: TLC7524
Other Parts Discussed in Thread: TL052, DAC8820
I want to use the TLC7524 to drive a TL052 op amp to generate a 20KHz square wave that ranges from -1v to 8v.
Here is my thought
Per the TLC7524
Vref -9v
Rfb +9v
Vdd 3.3v
Out2 to ground
Out1 is the output of the chip, it goes to input pin on TL052
CS tied to ground
WR controlled by 3.3v logic
D0-D7 driven by more 3.3v logic
TL052 used in non inverting with a 50k trim pot.
I need either a TINA file or a similar schematic as it seems that every time I try something new on a PCB without confirmation, there is trouble.
Thanks.
Regards