Part Number: ADC12DJ2700EVM
Other Parts Discussed in Thread: TSW14J57EVM
Hi Team,
My customer want to build up 4ch-2G simultaneous sampling system using our EVMs
As their starting point, they are considering to use following setup for 4ch-2G sampling now.
①ADC12DJ2700EVM→TSW14J57EVM→PC
②ADC12DJ2700EVM→TSW14J57EVM→PC
Then, They have some questions to realize the simultaneous sampling system.
1. Is it ok to connect the ADC12DJ2700EVM to the TSW14J56EVM also? Or should it be TSW14J57EVM?
2. How can we realize synchronization between ① and ②? Let me know if another EVM is needed for the sync.
3. Do you have any appnotes for the setups synchronization?
4. How long data can "ADC12DJ2700EVM → TSW14J57EVM → PC" setup capture at once?
(if possible, they also want to realize streaming capturing but it is impossible due to bus limitation of USB3.0)
Regards,
Takashi Onawa