Hi Team,
can ADS131A04`s charge pump power external device, like amps? if so what it`s maximum output current?
Thanks.
Regards, Sunny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sunny,
The ADS131A04's negative charge pump was designed to power a small negative rail just for the device, and not to power other devices. While there is a pin that requires a capacitor to supply charge, I don't know of any characterization data that shows it can drive an output load.
Joseph Wu
Sunny,
I was able to look at the output current of the negative charge pump with an ADS131A04EVM. With a dead short from the negative output to ground, the current was about 70uA. Again, that is with a short to ground and the output is 0V, not the normal -2V.
Based on that, I would guess that this output shouldn't be used to drive anything at all.
Joseph Wu