Hi,
I have programmed an ADC EVM using the TI ADC GUI to the following values:
0x211 OVR_T0 0xF2 (-0.5dB)
0x212 OVR_T1 0x1A (-19.87dB)
0x213 OVR_CFG 0xF (enable ovr, 111 samp period)
When I raise power levels in 0.1dB increments I do not see the OVR_T1 threshold trip until the OVR_T0 threshold is reached. At which point both are triggered. I can see this both with sticky bits from my firmware connected to the board and the orange LEDs that light up on the ADC EVM.
I have tried this with several OVR_T1 with the same results.
What could be causing this?
Thanks in advance,
Dan