Part Number: ADS124S06
Hi all,
we noticed a strange behaviour from ADS124S06. It seems that after a POWERDOWN command the device could not wake up anymore unless we send this command sequence:
STOP
WAKEUP
START
We want to powerdown the converter because we have two MCU that are reading the converter and the conversion result must be the same for both microcontrollers. So we think that we could obtain this behaviour if we powerdown the converter.
Are we missing something?
The converter is configured in this manner:
- pga bypassed
- continous conversions
- sample rate: 5 sps
- Reading from AIN4-AIN5
- Oscillator: internal
- Voltage reference: external (5Vd.c.)