Hi,
I want to keep ADC12DJ3200 in power down mode by default at power up by pulling up the PD pin high.
PD pin will be connected to FPGA and then FPGA will make the PD pin low when it wants the data from ADC.
But in datasheet it is written that power down using PD should not be used for long time.
So can we use PD pin for power down ADC at power up or is there any other method to keep ADC in power down or in reset mode?
Actually we will be using a custom GUI for our project and we want data from ADC to FPGA only when user selects the option in GUI.
So is there any method other than using PD, to stop ADC from sending digital data to FPGA?
An early response will be highly appreciated.
Thanks,
Lalit