I have a design using an ADS54J60 and Xilinx Kintex UltraScale FPGA. Need to determine the end to end latency.
I understand the latency from the sample to the serial output is 134 clocks + 4ns (refer to ADS54J60 datasheet figure 2). This parameter also appears to be tLAT-ADC as seen in TIDU171 figure 3.
Would seem that to be able to calculate the end to end latency the parameter tTX-LMFC needs to be known.
Has anyone else performed this calculation?
Any help would be appreciated.
Thanks, Gary