This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8900B: Single-ended bipolar to differential unipolar conversion

Part Number: ADS8900B
Other Parts Discussed in Thread: OPA625

Hi,

Is there an app note that shows the best parts to use to convert a single-ended bipolar signal to the 0-VREF differential unipolar input of the ADC?

The ADS8900B seems to be one of the lowest noise ADCs out there, but our application is measuring bio-potential signals that swing around ground.  Just checking if there is a particular circuit that is proven to do this for the ADS8900B before I start messing around with level translation (diff-amps with common mode).  Ideally, the solution is lower noise than the ADC itself (something like <5uV-RMS @ 8kHz bandwidth).

Thanks!

Erik