This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: Test ADS1299 with known sine wave signal

Part Number: ADS1299

Hi all,

I have developed my custom ADS1299 Board and till now have been successfully been able to read and write the registers. Also I have tested the ADS with its internal test signal and got a smooth square wave as output.

below are my register values and  internal test signal output excel sheet attached.

ADS1299-bridge has started!
111110
Register 0x1 modified.
----------------------------------------------
Register 0x2 modified.
Register 0x3 modified.
Register 0x15 modified.
Register 0x5 modified.
----------------------------------------------
ID  0x00  0x3E 0 0 1 1 1 1 1 0
CONFIG1  0x01  0xD6 1 1 0 1 0 1 1 0
CONFIG2  0x02  0xD0 1 1 0 1 0 0 0 0
CONFIG3  0x03  0xE0 1 1 1 0 0 0 0 0
LOFF  0x04  0x00 0 0 0 0 0 0 0 0
CH1SET  0x05  0x65 0 1 1 0 0 1 0 1
CH2SET  0x06  0x61 0 1 1 0 0 0 0 1
CH3SET  0x07  0x61 0 1 1 0 0 0 0 1
CH4SET  0x08  0x61 0 1 1 0 0 0 0 1
CH5SET  0x09  0x61 0 1 1 0 0 0 0 1
CH6SET  0x0A  0x61 0 1 1 0 0 0 0 1
CH7SET  0x0B  0x61 0 1 1 0 0 0 0 1
CH8SET  0x0C  0x61 0 1 1 0 0 0 0 1
BIAS_SENSP  0x0D  0x00 0 0 0 0 0 0 0 0
BIAS_SENSN  0x0E  0x00 0 0 0 0 0 0 0 0
LOFF_SENSP  0x0F  0x00 0 0 0 0 0 0 0 0
LOFF_SENSN  0x10  0x00 0 0 0 0 0 0 0 0
LOFF_FLIP  0x11  0x00 0 0 0 0 0 0 0 0
LOFF_STATP  0x12  0x00 0 0 0 0 0 0 0 0
LOFF_STATN  0x13  0x00 0 0 0 0 0 0 0 0
GPIO  0x14  0x0F 0 0 0 0 1 1 1 1
MISC1  0x15  0x20 0 0 1 0 0 0 0 0
MISC2  0x16  0x00 0 0 0 0 0 0 0 0
CONFIG4  0x17  0x00 0 0 0 0 0 0 0 0

Now I want to apply a sine wave from function generator before giving the actual EEG signal. Should I only change the Electrode mode to Normal Electrode Input for sine wave input or I need to change other Register Values too?EEG TEST ADS DATA.xlsx