This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8689: CONVERSION DATA READING ADDRESS

Part Number: ADS8689


unable to read the conversion data for ADS8689

Address for reading the conversion data

  • Hello A RAO,

    There is no address needed to read conversion data from this ADC,after the CONVST signal is sent to ADC and the conversion is done(tconv_max), the data will be shown on SDO with your SCLK signal.

    To identify and solve your issue, we need more information:

    • Your timing plot captured by a scope(CONVST/CS,SCLK,SDI and SDO)
    • Your schematic for review.
    • Your SPI configuration on CPU:     CPOL and CPHASE.

    Regards,

    Dale

  • It's hard to see, I only need one timing frame to check which should be similar as figure 3 or 4.

    Also,

    1. a capacitor(>4.7uF) is missed on REFIO pin. What's the measured voltage on REFIO pin?

    2. You are using different ground (GND and ISO_DGND) for AGND and DGND of ADS8689 ADC, where are they connected?

    3. What's your SPI configuration(CPOL and CPHASE) on CPU side? Did you change the setting in SDI_CTL_REG register of ADC?

    4. Did you see any signal on RVS pin before reading the code (/CS is high)?

    5. What's the analog input signal and what 's the code you got when you did the test?

    Regards,

    Dale