Part Number: AFE5818
Dear all,
I would like to ask the following questions.
[Question 1]
After turning on the power, the item to be set in the register of this IC is that the data sheet must be written to bits 2 and 4 in Section 10.4 (Initial Setup). Are there any other required items?
[Question 2]
There is a description such as Must Write 0 for the bit where the definition of the register of this IC is described, but there is no definition, but is it necessary to write even if it is the same as the Reset value? .
[Question 3]
Currently, the data sheet “SBAS687B-FEBRUARY 2015-REVISED AUGUST 2015” is being referenced. Can you tell me if there is any document that contains information about this IC other than "SBAS687B-FEBRUARY 2015-REVISED AUGUST 2015"?
(* For example, the setting value sequence is described)
Best Regards,
Y.Ottey