Part Number: ADS8028
Hi Expert,
My customer have an issue about temp sensor output value error at electromagnetic field immunity test.
Test : IEC61000-4-3 RI, 10V/m 80MHz
Temp sensor output value become unstable between 20C and 60C at electromagnetic field immunity test. (ADC values are stable)
Q1. Could you please let me know about internal circuit for Temp sensor? decupling cap, etc
It may be difficult to disclose the information. How do you think about the internal temp sensor to influence from EMC?
Q2. If they read the temp sensor value when TM_BUSY is low unintentionally, will the read results be unstable?
Thanks
Muk