This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC 4-20 mA or 4-20mA to 0-10V converter.

Hi everyone,

I need a converter 4-20mA to 0-10V or an ADC 4-20mA SPI or I2C. I would rather an ADC 4-20mA SPI or I2C than a 4-20mA to 0-10V or 0 - 5V converter.

I found this converter 4-20 mA to 0-5V but it is very old with only PDIP package, I would prefer something with EMC protection and so on.

Can anyone help me?

Best regards.