Other Parts Discussed in Thread: ADS1110, ADS1115, ADS1114
I have several questions on the TI ADS1110 ADC:
(1) I am trying to determine if negative offset readings for a single channel are typical for the ADS1110 ADC device.
The data in Decimal for 5 channels (starting with 1 in our numbering) is given below:
Chan1 Chan2 Chan3 Chan4 Chan5
14968 00015 00036 -00021 00015
Chan1 is loaded with 200kOhm resistor. All other channels are Open. All Open channels seem to have a positive offset except channel 4. Are negative offset possible? The signal conditioning circuitry is configured such that GND (0V) should be the minimum and all other voltages should be positive. Is this typical for this ADC, or should I be looking for leakage problems in the surrounding circuitry?
(2) Am I reading the ADC spec correctly? Is the ADC Resolution reduced from 16-bits to 12-bits for 240 Samples Per Second (or 240 SPS in the document)? If the Resolutions is reduced to 12-bit, is there a comparable ADC device which is 16-bit in the 250 SPS to 1000 SPS range? Preferably this would be a device which is still relatively low power consumption.