This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5560: ADS 5560 Data incorrect &output clk duty cycle is too large

Part Number: ADS5560


During the use of ads5560, it is found that the collected data value is incorrect and the duty cycle of the output CLK is also incorrect. The specific conditions are as follows:

1.Mode pin not connect , DFS pin voltage is 3 / 8 drvdd ,use 2s-complement data and parallel CMOS output

2. CLK input Refer to figure 53 of  specification,input clk duty cyele 50%

3. When input 0V, the ADC value collected is 15000, and the calculated value is - 0.4V. When input 1.5V DC level, the ADC value collected is 57000, which is converted into voltage value 1.2V

4.The duty cycle of output CLK is close to 90%

5.The output CLK duty cycle does not change when the Sen pin voltage is modified

  • Hi Chunqi lv,

    One of our device experts is looking into your questions, and will be back with you soon.

    Best Regards,

    Dan

  • Hi Chunqi lv,
    Sorry for the delay in my response due to holidays.

    What is the clock frequency you are using? 40MHz?

    Did you evaluate an ADS5560EVM or working on a custom board for you use-case?

    I can't think of a reason why the output clock duty cycle not 50%. Changing SEN pin voltage moves both positive edge and negative by same time period, so it won't affect the duty cycle.

    You mentioned that mode pin is not connected. Though this pin has an internal 100k ohm pull down, can you measure the voltage on that pin and make sure that it is 0V? Verify if grounding it helps.

    As you are trying to use parallel interface control only, is the RESET pin tied high?

    Regards,

    Vijay