Part Number: ADS54J42
Other Parts Discussed in Thread: ADS54J60, ADC32RF45
Hello,
My customer has a question about ADS54J42.
[Background]
This question is related with a following thread.
https://e2e.ti.com/support/data-converters/f/73/t/807324?tisearch=e2e-sitesearch&keymatch=ads54j42
They set the registers with 2021.ADS54J60_LMF_8224_2NQ.cfg in that thread.
Their configuration is as follows.
* Fs = 500MHz
* Input Frequency = 377MHz, LTE FDD 5MHz
Their test resust is as follows.
The part indicated by the circle is the spectrum that is not expected.
This is removed with CTRL NYQUIST = 0.
[Q]
Is there an appropriate order for "CTRL NYQUIST" and "NYQUIST ZONE" settings ?
You are instructed to set "NQ ZONE EN" before "NYQUIST ZONE" in ADC32RF45 D/S.
Do you know what the cause is ?
Please tell me the appropriate workaround.
Best Regards,
Hiroshi Katsunaga