I had help from a previous post and I thank you. I tried to make a close match TINA design to the TLC7524. The DB pins are driven manually instead of using 3.3v logic.
My pins of interest are VREF => +5v, VDD => +5v but not shown, OUT1, OUT2, and Rfb.
See picture. My TINA works well where the point at Rfb is negative and it can make the voltage value between R117(R3) and R123(R2) positive or negative.
By measuring resistance between OUT1 and Rfp on an unconnected, I measured 12K ohms. I then made the assumption for the rest of the R values.
I am having issues with the voltage values on my PCB at VF! and VF2 TLC7524.TSC - TINA.pdfTLC7524cc.TSCas if R14 is very much different. My voltage does not appear to follow the binary value of the DB pins. Will the drawing model I have of the resistor ladder give an accurate representation of the DC output of the TLC7524?