Part Number: ADS1248
Hello,
We are using ADS1248IPWR , Sigma-Delta ADC in one of our application.
Application details as follows,
1. Input range is 0-10V and -10 to +10V. With attenuation factor using voltage divider 0.085. i.e. when we provide 10V as input , output of voltage divider will be 0.85V.
2. Internal PGA gain is 2.
3. AVDD to ADC is 2.5V, AVSS is -2.5V and DVDD is 5V.
4. Used internal reference. i.e. 2.048V.
When we provide 20V as input then theoretically voltage divider output will be 1.7V. But, it is observed that at ADC input is around 1.38V and it is observed that ADC raw counts starts decreasing (Roll over) once ADC input voltage reached to 1.38Voltage.
Query 1:- What will be behaviour of ADS1248 when input voltage (Vin * PGA) rises above Internal reference 2.048V.
Query 2:- What will be behaviour of ADS1248 when input voltage (Vin * PGA) rises above AVDD (2.5V)
Query 3:- How to lock ADC counts when Input voltage rises above Reference voltage without count roll over.
Please do needful on high priority.
Thankyou for understanding.