Other Parts Discussed in Thread: ADS1262, ADS1220, ADS1248, ADS124S06
Dear Technical Support Team,
I'm investigating ADC as following specification.
Could you introduce the appropriate ADC product?
【requirement】
・MAX 4ch (1ch x4 or 4ch)
・measurement range : 50mV~950mV(-20~1000℃ with Platinel thermocouple)
・resolution(precision): 0.01℃
・measurement rate: 100ms(>10SPS)
・ENOB≧=22bit
・use Instrumentation amp
Best Regards,
ttd