This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RFEVM: Is sysref not required for on-board clock operation?

Part Number: ADC12DJ5200RFEVM


Hi,

I have a question regarding SYSREF when running the ADC12DJ5200RFEVM with the onboard clock.

I replaced the capacitor and resistor according to the user guide and set the clock source to on-board in EVMGUI, Fs = 5200 Msps, JMODE 1.

I was able to obtain the waveform of the sine wave input with this setting. However, in this configuration, the LMX's OUTB is powered down, and the SYSREF appears not to be input to the ADC.

To be honest, I'm not familiar with JESD, but I thought SYSREF was a must in subclass 1. Why does this ADC work?