Part Number: DAC43401
Other Parts Discussed in Thread: TPS61169
Hi DAC Team,
I am wondering if it is possible to use the DAC43401 as a square wave generator with an adjustable duty cycle. There is a use where the DAC would need to operate the PWM input of a LED driver, requiring >5kHz PWM signal with duty cycles from 0% to 100%.
Is this possible with the built in square wave generation? Is it possible to drive >5KHz outputs with these duty cycles?
Thanks!
Reed