Part Number: DAC7562T
Hi team,
what are the differences between DAC756xT and DAC756x?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Pengyu,
Thank you for your query. The difference between the DAC756xT and the DAC756x is the IO level. The part number with the suffix "T" supports 5V TTL IO level. That means the VIH (min) is
1. 2.1V for DAC756xT
2. (0.7*AVDD) for DAC756x
Hope that answers your question.
Regards,
Uttam Sahu
Applications Engineer, Precision DAC