This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45: S-parameters and SBAA219

Part Number: ADC32RF45

Hello,

I read the above Application Report regarding S-parameters for the ADC.

Q1. Page 6 states to use a 1:1 transformer to convert the differential impedance of the ADC input to single ended for the S-parameter model.  But the model is defined as differential by default; why is a transformer element is used? Is it the case that the measured impedance of ADC is single-ended?

Q2. Page 10.  The report state to use a 1:1 transformer to transformer but the ADS schematic uses 2:1 transformer.  Why is that? How is it calculated?

  • Hello,

    I downloaded the single-ended S-parameters from the forum related to ADC32RF45 and simulated the impedance.

    At 1.82GHz, the impedance (reference to 50 ohm) is 50*(0.216+j0.237) = 10.8+j11.85. Magnitude Z is about 16 ohm.  So for differential, the impedance is 2 times the Single Ended as 32 ohm differential (c.f. App Note, 25 ohm differential)

    Q1. Why is there a difference between the measured S-parameters and the App Note?

    Q2. Which one is correct?

  • Maxplus, 

    We are looking into your question and will get back to you asap. 

    Yusuf

  • Hi Maxplus,

    Q1. Page 6 states to use a 1:1 transformer to convert the differential impedance of the ADC input to single ended for the S-parameter model.  But the model is defined as differential by default; why is a transformer element is used? Is it the case that the measured impedance of ADC is single-ended?

    Ans: All S-parameters mentioned in the report are 'differential mode' quantities. To ease the understanding of the model, the 'DD' sufix is not added. SDD11 is mentioned as S11. The transformer element is used to get differential input from single ended S-parameter model. 

    Q2. Page 10.  The report state to use a 1:1 transformer to transformer but the ADS schematic uses 2:1 transformer.  Why is that? How is it calculated?

    Ans: The transformer used is 1:1 for each differential side. It is used here because differential 100 ohms reference is used here. This is explained in Figure 14. From Table 2, we can see what component values are used for differential 100 ohm (calculated from an assumed single ended 50 ohm system) 

    Regarding the mismatch between values from app note and S-parameter file provided, I have reached out to the team who made the app note. Will update you in 2 or 3 days.

    Regards,

    Vijay

  • Hi

    The s2p block of the ADC is measured in 50 ohm single ended. The reference differential impedance is 100 ohm for ADC. Therefore impedance transformer N should be 1.414.  Why is it to 2?

  • Hi Maxplus,

    Please find the attached differential S-parameters (S11dd) mentioned in the app-note. To design matching circuit, please use this file instead of the S2P block you downloaded earlier. For simulation, you can follow the method described in the app note as it is proven.

    freq	mag	angle	re	im
    1.00E+07	2.09E-01	-1.79E+02	-2.09E-01	-3.60E-03
    2.00E+07	1.98E-01	1.80E+02	-1.98E-01	1.12E-03
    3.00E+07	1.96E-01	-1.79E+02	-1.96E-01	-4.71E-03
    4.00E+07	2.10E-01	-1.76E+02	-2.10E-01	-1.49E-02
    5.00E+07	2.09E-01	-1.75E+02	-2.08E-01	-1.81E-02
    6.00E+07	2.10E-01	-1.74E+02	-2.09E-01	-2.19E-02
    7.00E+07	2.13E-01	-1.73E+02	-2.11E-01	-2.60E-02
    8.00E+07	2.13E-01	-1.72E+02	-2.11E-01	-2.95E-02
    9.00E+07	2.14E-01	-1.71E+02	-2.12E-01	-3.33E-02
    1.00E+08	2.17E-01	-1.70E+02	-2.14E-01	-3.72E-02
    1.10E+08	2.18E-01	-1.69E+02	-2.14E-01	-4.08E-02
    1.20E+08	2.19E-01	-1.68E+02	-2.15E-01	-4.46E-02
    1.30E+08	2.22E-01	-1.67E+02	-2.17E-01	-4.84E-02
    1.40E+08	2.23E-01	-1.66E+02	-2.17E-01	-5.22E-02
    1.50E+08	2.26E-01	-1.66E+02	-2.19E-01	-5.60E-02
    1.60E+08	2.29E-01	-1.65E+02	-2.21E-01	-5.97E-02
    1.70E+08	2.30E-01	-1.64E+02	-2.21E-01	-6.34E-02
    1.80E+08	2.33E-01	-1.63E+02	-2.23E-01	-6.70E-02
    1.90E+08	2.36E-01	-1.63E+02	-2.25E-01	-7.05E-02
    2.00E+08	2.38E-01	-1.62E+02	-2.26E-01	-7.42E-02
    2.10E+08	2.41E-01	-1.61E+02	-2.28E-01	-7.78E-02
    2.20E+08	2.44E-01	-1.61E+02	-2.31E-01	-8.13E-02
    2.30E+08	2.47E-01	-1.60E+02	-2.32E-01	-8.48E-02
    2.40E+08	2.50E-01	-1.59E+02	-2.34E-01	-8.82E-02
    2.50E+08	2.54E-01	-1.59E+02	-2.37E-01	-9.15E-02
    2.60E+08	2.57E-01	-1.58E+02	-2.38E-01	-9.49E-02
    2.70E+08	2.60E-01	-1.58E+02	-2.41E-01	-9.82E-02
    2.80E+08	2.64E-01	-1.57E+02	-2.43E-01	-1.02E-01
    2.90E+08	2.67E-01	-1.57E+02	-2.45E-01	-1.05E-01
    3.00E+08	2.71E-01	-1.56E+02	-2.48E-01	-1.09E-01
    3.10E+08	2.75E-01	-1.56E+02	-2.51E-01	-1.12E-01
    3.20E+08	2.78E-01	-1.56E+02	-2.53E-01	-1.15E-01
    3.30E+08	2.82E-01	-1.55E+02	-2.56E-01	-1.19E-01
    3.40E+08	2.86E-01	-1.55E+02	-2.59E-01	-1.22E-01
    3.50E+08	2.90E-01	-1.54E+02	-2.62E-01	-1.25E-01
    3.60E+08	2.94E-01	-1.54E+02	-2.65E-01	-1.28E-01
    3.70E+08	2.98E-01	-1.54E+02	-2.68E-01	-1.31E-01
    3.80E+08	3.02E-01	-1.54E+02	-2.70E-01	-1.34E-01
    3.90E+08	3.06E-01	-1.53E+02	-2.73E-01	-1.37E-01
    4.00E+08	3.10E-01	-1.53E+02	-2.77E-01	-1.39E-01
    4.10E+08	3.14E-01	-1.53E+02	-2.80E-01	-1.42E-01
    4.20E+08	3.18E-01	-1.53E+02	-2.83E-01	-1.45E-01
    4.30E+08	3.23E-01	-1.53E+02	-2.87E-01	-1.48E-01
    4.40E+08	3.27E-01	-1.53E+02	-2.90E-01	-1.50E-01
    4.50E+08	3.31E-01	-1.52E+02	-2.94E-01	-1.53E-01
    4.60E+08	3.36E-01	-1.52E+02	-2.98E-01	-1.56E-01
    4.70E+08	3.40E-01	-1.52E+02	-3.01E-01	-1.58E-01
    4.80E+08	3.45E-01	-1.52E+02	-3.05E-01	-1.60E-01
    4.90E+08	3.50E-01	-1.52E+02	-3.09E-01	-1.63E-01
    5.00E+08	3.54E-01	-1.52E+02	-3.13E-01	-1.65E-01
    5.10E+08	3.58E-01	-1.52E+02	-3.16E-01	-1.68E-01
    5.20E+08	3.63E-01	-1.52E+02	-3.20E-01	-1.70E-01
    5.30E+08	3.67E-01	-1.52E+02	-3.24E-01	-1.72E-01
    5.40E+08	3.71E-01	-1.52E+02	-3.28E-01	-1.75E-01
    5.50E+08	3.76E-01	-1.52E+02	-3.32E-01	-1.77E-01
    5.60E+08	3.80E-01	-1.52E+02	-3.36E-01	-1.78E-01
    5.70E+08	3.85E-01	-1.52E+02	-3.40E-01	-1.80E-01
    5.80E+08	3.89E-01	-1.52E+02	-3.44E-01	-1.82E-01
    5.90E+08	3.94E-01	-1.52E+02	-3.48E-01	-1.83E-01
    6.00E+08	3.98E-01	-1.52E+02	-3.53E-01	-1.85E-01
    6.10E+08	4.03E-01	-1.52E+02	-3.57E-01	-1.87E-01
    6.20E+08	4.08E-01	-1.53E+02	-3.61E-01	-1.88E-01
    6.30E+08	4.12E-01	-1.53E+02	-3.66E-01	-1.90E-01
    6.40E+08	4.17E-01	-1.53E+02	-3.71E-01	-1.91E-01
    6.50E+08	4.21E-01	-1.53E+02	-3.75E-01	-1.92E-01
    6.60E+08	4.26E-01	-1.53E+02	-3.79E-01	-1.94E-01
    6.70E+08	4.31E-01	-1.53E+02	-3.84E-01	-1.95E-01
    6.80E+08	4.35E-01	-1.53E+02	-3.88E-01	-1.96E-01
    6.90E+08	4.39E-01	-1.53E+02	-3.93E-01	-1.97E-01
    7.00E+08	4.44E-01	-1.53E+02	-3.97E-01	-1.98E-01
    7.10E+08	4.48E-01	-1.54E+02	-4.01E-01	-1.99E-01
    7.20E+08	4.53E-01	-1.54E+02	-4.06E-01	-2.00E-01
    7.30E+08	4.57E-01	-1.54E+02	-4.11E-01	-2.01E-01
    7.40E+08	4.61E-01	-1.54E+02	-4.15E-01	-2.01E-01
    7.50E+08	4.65E-01	-1.54E+02	-4.19E-01	-2.02E-01
    7.60E+08	4.70E-01	-1.55E+02	-4.24E-01	-2.02E-01
    7.70E+08	4.74E-01	-1.55E+02	-4.28E-01	-2.03E-01
    7.80E+08	4.78E-01	-1.55E+02	-4.33E-01	-2.03E-01
    7.90E+08	4.83E-01	-1.55E+02	-4.38E-01	-2.03E-01
    8.00E+08	4.87E-01	-1.55E+02	-4.42E-01	-2.04E-01
    8.10E+08	4.91E-01	-1.56E+02	-4.47E-01	-2.04E-01
    8.20E+08	4.96E-01	-1.56E+02	-4.52E-01	-2.04E-01
    8.30E+08	5.00E-01	-1.56E+02	-4.56E-01	-2.03E-01
    8.40E+08	5.04E-01	-1.56E+02	-4.61E-01	-2.03E-01
    8.50E+08	5.08E-01	-1.56E+02	-4.66E-01	-2.03E-01
    8.60E+08	5.12E-01	-1.57E+02	-4.70E-01	-2.03E-01
    8.70E+08	5.16E-01	-1.57E+02	-4.74E-01	-2.03E-01
    8.80E+08	5.20E-01	-1.57E+02	-4.79E-01	-2.02E-01
    8.90E+08	5.24E-01	-1.57E+02	-4.83E-01	-2.02E-01
    9.00E+08	5.28E-01	-1.58E+02	-4.88E-01	-2.02E-01
    9.10E+08	5.32E-01	-1.58E+02	-4.92E-01	-2.01E-01
    9.20E+08	5.36E-01	-1.58E+02	-4.97E-01	-2.00E-01
    9.30E+08	5.39E-01	-1.58E+02	-5.01E-01	-1.99E-01
    9.40E+08	5.43E-01	-1.59E+02	-5.06E-01	-1.98E-01
    9.50E+08	5.47E-01	-1.59E+02	-5.10E-01	-1.97E-01
    9.60E+08	5.51E-01	-1.59E+02	-5.15E-01	-1.96E-01
    9.70E+08	5.55E-01	-1.59E+02	-5.19E-01	-1.95E-01
    9.80E+08	5.58E-01	-1.60E+02	-5.23E-01	-1.93E-01
    9.90E+08	5.61E-01	-1.60E+02	-5.28E-01	-1.92E-01
    1.00E+09	5.65E-01	-1.60E+02	-5.32E-01	-1.91E-01
    1.01E+09	5.68E-01	-1.60E+02	-5.36E-01	-1.90E-01
    1.02E+09	5.72E-01	-1.61E+02	-5.40E-01	-1.88E-01
    1.03E+09	5.76E-01	-1.61E+02	-5.44E-01	-1.87E-01
    1.04E+09	5.79E-01	-1.61E+02	-5.49E-01	-1.86E-01
    1.05E+09	5.83E-01	-1.62E+02	-5.53E-01	-1.84E-01
    1.06E+09	5.86E-01	-1.62E+02	-5.57E-01	-1.83E-01
    1.07E+09	5.89E-01	-1.62E+02	-5.61E-01	-1.81E-01
    1.08E+09	5.93E-01	-1.62E+02	-5.65E-01	-1.79E-01
    1.09E+09	5.96E-01	-1.63E+02	-5.69E-01	-1.77E-01
    1.10E+09	5.99E-01	-1.63E+02	-5.73E-01	-1.75E-01
    1.11E+09	6.02E-01	-1.63E+02	-5.77E-01	-1.73E-01
    1.12E+09	6.05E-01	-1.64E+02	-5.81E-01	-1.71E-01
    1.13E+09	6.08E-01	-1.64E+02	-5.84E-01	-1.69E-01
    1.14E+09	6.12E-01	-1.64E+02	-5.88E-01	-1.67E-01
    1.15E+09	6.15E-01	-1.64E+02	-5.92E-01	-1.65E-01
    1.16E+09	6.18E-01	-1.65E+02	-5.96E-01	-1.63E-01
    1.17E+09	6.21E-01	-1.65E+02	-6.00E-01	-1.61E-01
    1.18E+09	6.24E-01	-1.65E+02	-6.04E-01	-1.59E-01
    1.19E+09	6.27E-01	-1.66E+02	-6.07E-01	-1.57E-01
    1.20E+09	6.30E-01	-1.66E+02	-6.11E-01	-1.55E-01
    1.21E+09	6.33E-01	-1.66E+02	-6.14E-01	-1.52E-01
    1.22E+09	6.36E-01	-1.66E+02	-6.18E-01	-1.50E-01
    1.23E+09	6.38E-01	-1.67E+02	-6.21E-01	-1.48E-01
    1.24E+09	6.41E-01	-1.67E+02	-6.24E-01	-1.45E-01
    1.25E+09	6.43E-01	-1.67E+02	-6.27E-01	-1.42E-01
    1.26E+09	6.46E-01	-1.68E+02	-6.31E-01	-1.40E-01
    1.27E+09	6.48E-01	-1.68E+02	-6.34E-01	-1.37E-01
    1.28E+09	6.51E-01	-1.68E+02	-6.37E-01	-1.34E-01
    1.29E+09	6.54E-01	-1.68E+02	-6.40E-01	-1.32E-01
    1.30E+09	6.57E-01	-1.69E+02	-6.44E-01	-1.29E-01
    1.31E+09	6.59E-01	-1.69E+02	-6.47E-01	-1.27E-01
    1.32E+09	6.62E-01	-1.69E+02	-6.50E-01	-1.24E-01
    1.33E+09	6.64E-01	-1.69E+02	-6.53E-01	-1.22E-01
    1.34E+09	6.67E-01	-1.70E+02	-6.56E-01	-1.19E-01
    1.35E+09	6.69E-01	-1.70E+02	-6.59E-01	-1.17E-01
    1.36E+09	6.71E-01	-1.70E+02	-6.62E-01	-1.14E-01
    1.37E+09	6.74E-01	-1.70E+02	-6.64E-01	-1.12E-01
    1.38E+09	6.76E-01	-1.71E+02	-6.67E-01	-1.09E-01
    1.39E+09	6.78E-01	-1.71E+02	-6.69E-01	-1.07E-01
    1.40E+09	6.80E-01	-1.71E+02	-6.72E-01	-1.04E-01
    1.41E+09	6.82E-01	-1.71E+02	-6.74E-01	-1.01E-01
    1.42E+09	6.84E-01	-1.72E+02	-6.77E-01	-9.80E-02
    1.43E+09	6.86E-01	-1.72E+02	-6.79E-01	-9.53E-02
    1.44E+09	6.88E-01	-1.72E+02	-6.82E-01	-9.25E-02
    1.45E+09	6.90E-01	-1.73E+02	-6.85E-01	-8.98E-02
    1.46E+09	6.92E-01	-1.73E+02	-6.87E-01	-8.69E-02
    1.47E+09	6.94E-01	-1.73E+02	-6.89E-01	-8.40E-02
    1.48E+09	6.96E-01	-1.73E+02	-6.91E-01	-8.13E-02
    1.49E+09	6.98E-01	-1.74E+02	-6.93E-01	-7.90E-02
    1.50E+09	7.00E-01	-1.74E+02	-6.96E-01	-7.67E-02
    1.51E+09	7.02E-01	-1.74E+02	-6.98E-01	-7.44E-02
    1.52E+09	7.04E-01	-1.74E+02	-7.00E-01	-7.20E-02
    1.53E+09	7.05E-01	-1.74E+02	-7.02E-01	-6.97E-02
    1.54E+09	7.07E-01	-1.75E+02	-7.04E-01	-6.72E-02
    1.55E+09	7.09E-01	-1.75E+02	-7.06E-01	-6.46E-02
    1.56E+09	7.10E-01	-1.75E+02	-7.08E-01	-6.19E-02
    1.57E+09	7.12E-01	-1.75E+02	-7.10E-01	-5.92E-02
    1.58E+09	7.14E-01	-1.75E+02	-7.11E-01	-5.63E-02
    1.59E+09	7.15E-01	-1.76E+02	-7.13E-01	-5.33E-02
    1.60E+09	7.17E-01	-1.76E+02	-7.15E-01	-5.04E-02
    1.61E+09	7.18E-01	-1.76E+02	-7.17E-01	-4.75E-02
    1.62E+09	7.20E-01	-1.76E+02	-7.18E-01	-4.47E-02
    1.63E+09	7.21E-01	-1.77E+02	-7.20E-01	-4.19E-02
    1.64E+09	7.23E-01	-1.77E+02	-7.22E-01	-3.95E-02
    1.65E+09	7.24E-01	-1.77E+02	-7.24E-01	-3.70E-02
    1.66E+09	7.26E-01	-1.77E+02	-7.25E-01	-3.46E-02
    1.67E+09	7.27E-01	-1.77E+02	-7.27E-01	-3.24E-02
    1.68E+09	7.29E-01	-1.78E+02	-7.28E-01	-3.02E-02
    1.69E+09	7.30E-01	-1.78E+02	-7.30E-01	-2.79E-02
    1.70E+09	7.31E-01	-1.78E+02	-7.31E-01	-2.57E-02
    1.71E+09	7.33E-01	-1.78E+02	-7.32E-01	-2.35E-02
    1.72E+09	7.34E-01	-1.78E+02	-7.34E-01	-2.13E-02
    1.73E+09	7.35E-01	-1.79E+02	-7.34E-01	-1.89E-02
    1.74E+09	7.35E-01	-1.79E+02	-7.35E-01	-1.65E-02
    1.75E+09	7.36E-01	-1.79E+02	-7.36E-01	-1.41E-02
    1.76E+09	7.37E-01	-1.79E+02	-7.37E-01	-1.16E-02
    1.77E+09	7.38E-01	-1.79E+02	-7.38E-01	-9.14E-03
    1.78E+09	7.39E-01	-1.79E+02	-7.39E-01	-6.63E-03
    1.79E+09	7.40E-01	-1.80E+02	-7.40E-01	-4.14E-03
    1.80E+09	7.41E-01	-1.80E+02	-7.41E-01	-1.63E-03
    1.81E+09	7.43E-01	1.80E+02	-7.43E-01	8.31E-04
    1.82E+09	7.44E-01	1.80E+02	-7.44E-01	3.11E-03
    1.83E+09	7.45E-01	1.80E+02	-7.45E-01	5.42E-03
    1.84E+09	7.46E-01	1.79E+02	-7.46E-01	7.58E-03
    1.85E+09	7.47E-01	1.79E+02	-7.47E-01	9.35E-03
    1.86E+09	7.48E-01	1.79E+02	-7.48E-01	1.11E-02
    1.87E+09	7.49E-01	1.79E+02	-7.49E-01	1.29E-02
    1.88E+09	7.49E-01	1.79E+02	-7.49E-01	1.46E-02
    1.89E+09	7.50E-01	1.79E+02	-7.50E-01	1.63E-02
    1.90E+09	7.50E-01	1.79E+02	-7.50E-01	1.80E-02
    1.91E+09	7.51E-01	1.78E+02	-7.51E-01	1.99E-02
    1.92E+09	7.52E-01	1.78E+02	-7.51E-01	2.18E-02
    1.93E+09	7.52E-01	1.78E+02	-7.52E-01	2.38E-02
    1.94E+09	7.53E-01	1.78E+02	-7.52E-01	2.63E-02
    1.95E+09	7.53E-01	1.78E+02	-7.53E-01	2.88E-02
    1.96E+09	7.54E-01	1.78E+02	-7.53E-01	3.13E-02
    1.97E+09	7.55E-01	1.77E+02	-7.54E-01	3.40E-02
    1.98E+09	7.55E-01	1.77E+02	-7.54E-01	3.67E-02
    1.99E+09	7.56E-01	1.77E+02	-7.55E-01	3.92E-02
    2.00E+09	7.56E-01	1.77E+02	-7.55E-01	4.12E-02
    2.01E+09	7.57E-01	1.77E+02	-7.56E-01	4.32E-02
    2.02E+09	7.57E-01	1.77E+02	-7.56E-01	4.50E-02
    2.03E+09	7.58E-01	1.76E+02	-7.56E-01	4.65E-02
    2.04E+09	7.58E-01	1.76E+02	-7.57E-01	4.79E-02
    2.05E+09	7.58E-01	1.76E+02	-7.57E-01	4.94E-02
    2.06E+09	7.59E-01	1.76E+02	-7.57E-01	5.09E-02
    2.07E+09	7.60E-01	1.76E+02	-7.58E-01	5.25E-02
    2.08E+09	7.60E-01	1.76E+02	-7.58E-01	5.43E-02
    2.09E+09	7.60E-01	1.76E+02	-7.58E-01	5.67E-02
    2.10E+09	7.60E-01	1.76E+02	-7.58E-01	5.90E-02
    2.11E+09	7.60E-01	1.75E+02	-7.58E-01	6.14E-02
    2.12E+09	7.60E-01	1.75E+02	-7.57E-01	6.38E-02
    2.13E+09	7.60E-01	1.75E+02	-7.57E-01	6.63E-02
    2.14E+09	7.60E-01	1.75E+02	-7.57E-01	6.87E-02
    2.15E+09	7.60E-01	1.75E+02	-7.57E-01	7.10E-02
    2.16E+09	7.60E-01	1.74E+02	-7.57E-01	7.34E-02
    2.17E+09	7.61E-01	1.74E+02	-7.57E-01	7.56E-02
    2.18E+09	7.61E-01	1.74E+02	-7.57E-01	7.74E-02
    2.19E+09	7.61E-01	1.74E+02	-7.57E-01	7.93E-02
    2.20E+09	7.61E-01	1.74E+02	-7.57E-01	8.11E-02
    2.21E+09	7.61E-01	1.74E+02	-7.57E-01	8.29E-02
    2.22E+09	7.62E-01	1.74E+02	-7.57E-01	8.48E-02
    2.23E+09	7.62E-01	1.73E+02	-7.57E-01	8.66E-02
    2.24E+09	7.62E-01	1.73E+02	-7.56E-01	8.85E-02
    2.25E+09	7.61E-01	1.73E+02	-7.56E-01	9.05E-02
    2.26E+09	7.61E-01	1.73E+02	-7.55E-01	9.25E-02
    2.27E+09	7.61E-01	1.73E+02	-7.55E-01	9.50E-02
    2.28E+09	7.60E-01	1.73E+02	-7.54E-01	9.74E-02
    2.29E+09	7.60E-01	1.72E+02	-7.53E-01	9.97E-02
    2.30E+09	7.60E-01	1.72E+02	-7.53E-01	1.02E-01
    2.31E+09	7.60E-01	1.72E+02	-7.53E-01	1.04E-01
    2.32E+09	7.60E-01	1.72E+02	-7.52E-01	1.07E-01
    2.33E+09	7.60E-01	1.72E+02	-7.52E-01	1.09E-01
    2.34E+09	7.60E-01	1.72E+02	-7.52E-01	1.12E-01
    2.35E+09	7.60E-01	1.71E+02	-7.51E-01	1.14E-01
    2.36E+09	7.60E-01	1.71E+02	-7.51E-01	1.16E-01
    2.37E+09	7.60E-01	1.71E+02	-7.50E-01	1.18E-01
    2.38E+09	7.59E-01	1.71E+02	-7.50E-01	1.20E-01
    2.39E+09	7.59E-01	1.71E+02	-7.49E-01	1.22E-01
    2.40E+09	7.58E-01	1.71E+02	-7.48E-01	1.24E-01
    2.41E+09	7.57E-01	1.70E+02	-7.47E-01	1.27E-01
    2.42E+09	7.57E-01	1.70E+02	-7.46E-01	1.29E-01
    2.43E+09	7.56E-01	1.70E+02	-7.45E-01	1.31E-01
    2.44E+09	7.56E-01	1.70E+02	-7.44E-01	1.33E-01
    2.45E+09	7.55E-01	1.70E+02	-7.43E-01	1.36E-01
    2.46E+09	7.55E-01	1.69E+02	-7.42E-01	1.38E-01
    2.47E+09	7.55E-01	1.69E+02	-7.42E-01	1.41E-01
    2.48E+09	7.55E-01	1.69E+02	-7.41E-01	1.43E-01
    2.49E+09	7.54E-01	1.69E+02	-7.40E-01	1.46E-01
    2.50E+09	7.54E-01	1.69E+02	-7.39E-01	1.49E-01
    2.51E+09	7.54E-01	1.68E+02	-7.38E-01	1.51E-01
    2.52E+09	7.53E-01	1.68E+02	-7.37E-01	1.53E-01
    2.53E+09	7.53E-01	1.68E+02	-7.37E-01	1.55E-01
    2.54E+09	7.52E-01	1.68E+02	-7.36E-01	1.57E-01
    2.55E+09	7.51E-01	1.68E+02	-7.34E-01	1.59E-01
    2.56E+09	7.51E-01	1.68E+02	-7.33E-01	1.61E-01
    2.57E+09	7.50E-01	1.67E+02	-7.32E-01	1.63E-01
    2.58E+09	7.50E-01	1.67E+02	-7.31E-01	1.65E-01
    2.59E+09	7.49E-01	1.67E+02	-7.30E-01	1.67E-01
    2.60E+09	7.49E-01	1.67E+02	-7.29E-01	1.70E-01
    2.61E+09	7.49E-01	1.67E+02	-7.28E-01	1.72E-01
    2.62E+09	7.48E-01	1.66E+02	-7.27E-01	1.75E-01
    2.63E+09	7.47E-01	1.66E+02	-7.26E-01	1.78E-01
    2.64E+09	7.47E-01	1.66E+02	-7.24E-01	1.81E-01
    2.65E+09	7.46E-01	1.66E+02	-7.23E-01	1.84E-01
    2.66E+09	7.45E-01	1.66E+02	-7.22E-01	1.86E-01
    2.67E+09	7.45E-01	1.65E+02	-7.21E-01	1.89E-01
    2.68E+09	7.44E-01	1.65E+02	-7.20E-01	1.91E-01
    2.69E+09	7.44E-01	1.65E+02	-7.19E-01	1.92E-01
    2.70E+09	7.44E-01	1.65E+02	-7.18E-01	1.94E-01
    2.71E+09	7.43E-01	1.65E+02	-7.17E-01	1.96E-01
    2.72E+09	7.43E-01	1.65E+02	-7.16E-01	1.98E-01
    2.73E+09	7.42E-01	1.64E+02	-7.15E-01	1.99E-01
    2.74E+09	7.42E-01	1.64E+02	-7.14E-01	2.01E-01
    2.75E+09	7.41E-01	1.64E+02	-7.12E-01	2.04E-01
    2.76E+09	7.40E-01	1.64E+02	-7.11E-01	2.06E-01
    2.77E+09	7.39E-01	1.64E+02	-7.09E-01	2.08E-01
    2.78E+09	7.38E-01	1.63E+02	-7.07E-01	2.10E-01
    2.79E+09	7.37E-01	1.63E+02	-7.06E-01	2.13E-01
    2.80E+09	7.36E-01	1.63E+02	-7.04E-01	2.15E-01
    2.81E+09	7.36E-01	1.63E+02	-7.03E-01	2.17E-01
    2.82E+09	7.35E-01	1.63E+02	-7.01E-01	2.20E-01
    2.83E+09	7.35E-01	1.62E+02	-7.00E-01	2.22E-01
    2.84E+09	7.34E-01	1.62E+02	-6.99E-01	2.24E-01
    2.85E+09	7.34E-01	1.62E+02	-6.98E-01	2.26E-01
    2.86E+09	7.33E-01	1.62E+02	-6.97E-01	2.28E-01
    2.87E+09	7.33E-01	1.62E+02	-6.96E-01	2.29E-01
    2.88E+09	7.33E-01	1.62E+02	-6.95E-01	2.30E-01
    2.89E+09	7.32E-01	1.62E+02	-6.94E-01	2.32E-01
    2.90E+09	7.31E-01	1.61E+02	-6.93E-01	2.33E-01
    2.91E+09	7.30E-01	1.61E+02	-6.92E-01	2.34E-01
    2.92E+09	7.29E-01	1.61E+02	-6.90E-01	2.35E-01
    2.93E+09	7.28E-01	1.61E+02	-6.88E-01	2.37E-01
    2.94E+09	7.27E-01	1.61E+02	-6.87E-01	2.38E-01
    2.95E+09	7.26E-01	1.61E+02	-6.85E-01	2.40E-01
    2.96E+09	7.25E-01	1.61E+02	-6.83E-01	2.42E-01
    2.97E+09	7.24E-01	1.60E+02	-6.81E-01	2.44E-01
    2.98E+09	7.23E-01	1.60E+02	-6.80E-01	2.46E-01
    2.99E+09	7.22E-01	1.60E+02	-6.78E-01	2.48E-01
    3.00E+09	7.21E-01	1.60E+02	-6.76E-01	2.51E-01
    3.01E+09	7.21E-01	1.59E+02	-6.75E-01	2.53E-01
    3.02E+09	7.20E-01	1.59E+02	-6.74E-01	2.55E-01
    3.03E+09	7.20E-01	1.59E+02	-6.73E-01	2.56E-01
    3.04E+09	7.19E-01	1.59E+02	-6.72E-01	2.57E-01
    3.05E+09	7.18E-01	1.59E+02	-6.71E-01	2.58E-01
    3.06E+09	7.18E-01	1.59E+02	-6.69E-01	2.58E-01
    3.07E+09	7.17E-01	1.59E+02	-6.69E-01	2.59E-01
    3.08E+09	7.17E-01	1.59E+02	-6.68E-01	2.59E-01
    3.09E+09	7.16E-01	1.59E+02	-6.67E-01	2.60E-01
    3.10E+09	7.16E-01	1.59E+02	-6.66E-01	2.61E-01
    3.11E+09	7.15E-01	1.58E+02	-6.65E-01	2.63E-01
    3.12E+09	7.14E-01	1.58E+02	-6.63E-01	2.65E-01
    3.13E+09	7.13E-01	1.58E+02	-6.61E-01	2.68E-01
    3.14E+09	7.11E-01	1.58E+02	-6.57E-01	2.71E-01
    3.15E+09	7.09E-01	1.57E+02	-6.54E-01	2.74E-01
    3.16E+09	7.08E-01	1.57E+02	-6.51E-01	2.76E-01
    3.17E+09	7.06E-01	1.57E+02	-6.49E-01	2.79E-01
    3.18E+09	7.04E-01	1.56E+02	-6.46E-01	2.81E-01
    3.19E+09	7.03E-01	1.56E+02	-6.43E-01	2.83E-01
    3.20E+09	7.02E-01	1.56E+02	-6.41E-01	2.84E-01
    3.21E+09	7.00E-01	1.56E+02	-6.39E-01	2.86E-01
    3.22E+09	6.99E-01	1.56E+02	-6.38E-01	2.86E-01
    3.23E+09	6.98E-01	1.56E+02	-6.37E-01	2.87E-01
    3.24E+09	6.97E-01	1.56E+02	-6.35E-01	2.87E-01
    3.25E+09	6.96E-01	1.56E+02	-6.33E-01	2.88E-01
    3.26E+09	6.94E-01	1.55E+02	-6.31E-01	2.89E-01
    3.27E+09	6.92E-01	1.55E+02	-6.29E-01	2.90E-01
    3.28E+09	6.90E-01	1.55E+02	-6.26E-01	2.91E-01
    3.29E+09	6.89E-01	1.55E+02	-6.23E-01	2.93E-01
    3.30E+09	6.87E-01	1.55E+02	-6.20E-01	2.95E-01
    3.31E+09	6.84E-01	1.54E+02	-6.17E-01	2.97E-01
    3.32E+09	6.82E-01	1.54E+02	-6.13E-01	2.99E-01
    3.33E+09	6.80E-01	1.54E+02	-6.10E-01	3.01E-01
    3.34E+09	6.78E-01	1.53E+02	-6.06E-01	3.03E-01
    3.35E+09	6.77E-01	1.53E+02	-6.04E-01	3.06E-01
    3.36E+09	6.75E-01	1.53E+02	-6.01E-01	3.08E-01
    3.37E+09	6.74E-01	1.53E+02	-5.98E-01	3.10E-01
    3.38E+09	6.73E-01	1.52E+02	-5.96E-01	3.13E-01
    3.39E+09	6.72E-01	1.52E+02	-5.94E-01	3.15E-01
    3.40E+09	6.71E-01	1.52E+02	-5.92E-01	3.17E-01
    3.41E+09	6.69E-01	1.52E+02	-5.89E-01	3.18E-01
    3.42E+09	6.67E-01	1.51E+02	-5.86E-01	3.20E-01
    3.43E+09	6.65E-01	1.51E+02	-5.83E-01	3.21E-01
    3.44E+09	6.63E-01	1.51E+02	-5.79E-01	3.22E-01
    3.45E+09	6.60E-01	1.51E+02	-5.75E-01	3.23E-01
    3.46E+09	6.57E-01	1.50E+02	-5.71E-01	3.25E-01
    3.47E+09	6.55E-01	1.50E+02	-5.67E-01	3.27E-01
    3.48E+09	6.52E-01	1.50E+02	-5.63E-01	3.29E-01
    3.49E+09	6.50E-01	1.49E+02	-5.59E-01	3.31E-01
    3.50E+09	6.47E-01	1.49E+02	-5.55E-01	3.33E-01
    3.51E+09	6.45E-01	1.49E+02	-5.51E-01	3.36E-01
    3.52E+09	6.43E-01	1.48E+02	-5.47E-01	3.39E-01
    3.53E+09	6.42E-01	1.48E+02	-5.43E-01	3.42E-01
    3.54E+09	6.40E-01	1.47E+02	-5.39E-01	3.45E-01
    3.55E+09	6.38E-01	1.47E+02	-5.35E-01	3.48E-01
    3.56E+09	6.36E-01	1.47E+02	-5.32E-01	3.49E-01
    3.57E+09	6.34E-01	1.46E+02	-5.28E-01	3.51E-01
    3.58E+09	6.32E-01	1.46E+02	-5.25E-01	3.52E-01
    3.59E+09	6.31E-01	1.46E+02	-5.22E-01	3.54E-01
    3.60E+09	6.29E-01	1.46E+02	-5.19E-01	3.55E-01
    3.61E+09	6.27E-01	1.45E+02	-5.16E-01	3.56E-01
    3.62E+09	6.25E-01	1.45E+02	-5.12E-01	3.58E-01
    3.63E+09	6.23E-01	1.45E+02	-5.08E-01	3.59E-01
    3.64E+09	6.20E-01	1.44E+02	-5.04E-01	3.62E-01
    3.65E+09	6.18E-01	1.44E+02	-4.99E-01	3.64E-01
    3.66E+09	6.16E-01	1.43E+02	-4.94E-01	3.67E-01
    3.67E+09	6.13E-01	1.43E+02	-4.89E-01	3.70E-01
    3.68E+09	6.11E-01	1.42E+02	-4.84E-01	3.73E-01
    3.69E+09	6.09E-01	1.42E+02	-4.79E-01	3.76E-01
    3.70E+09	6.07E-01	1.41E+02	-4.74E-01	3.79E-01
    3.71E+09	6.05E-01	1.41E+02	-4.70E-01	3.81E-01
    3.72E+09	6.03E-01	1.41E+02	-4.65E-01	3.84E-01
    3.73E+09	6.01E-01	1.40E+02	-4.61E-01	3.86E-01
    3.74E+09	6.00E-01	1.40E+02	-4.58E-01	3.88E-01
    3.75E+09	5.99E-01	1.39E+02	-4.54E-01	3.90E-01
    3.76E+09	5.97E-01	1.39E+02	-4.51E-01	3.92E-01
    3.77E+09	5.96E-01	1.39E+02	-4.48E-01	3.93E-01
    3.78E+09	5.95E-01	1.38E+02	-4.45E-01	3.95E-01
    3.79E+09	5.93E-01	1.38E+02	-4.40E-01	3.97E-01
    3.80E+09	5.91E-01	1.38E+02	-4.36E-01	3.99E-01
    3.81E+09	5.88E-01	1.37E+02	-4.31E-01	4.00E-01
    3.82E+09	5.86E-01	1.37E+02	-4.26E-01	4.02E-01
    3.83E+09	5.84E-01	1.36E+02	-4.21E-01	4.05E-01
    3.84E+09	5.82E-01	1.36E+02	-4.16E-01	4.07E-01
    3.85E+09	5.80E-01	1.35E+02	-4.11E-01	4.09E-01
    3.86E+09	5.79E-01	1.35E+02	-4.06E-01	4.12E-01
    3.87E+09	5.77E-01	1.34E+02	-4.01E-01	4.15E-01
    3.88E+09	5.76E-01	1.34E+02	-3.97E-01	4.18E-01
    3.89E+09	5.76E-01	1.33E+02	-3.93E-01	4.21E-01
    3.90E+09	5.76E-01	1.33E+02	-3.90E-01	4.24E-01
    3.91E+09	5.75E-01	1.32E+02	-3.86E-01	4.26E-01
    3.92E+09	5.75E-01	1.32E+02	-3.83E-01	4.29E-01
    3.93E+09	5.75E-01	1.31E+02	-3.80E-01	4.31E-01
    3.94E+09	5.74E-01	1.31E+02	-3.76E-01	4.33E-01
    3.95E+09	5.73E-01	1.31E+02	-3.73E-01	4.35E-01
    3.96E+09	5.72E-01	1.30E+02	-3.69E-01	4.36E-01
    3.97E+09	5.70E-01	1.30E+02	-3.66E-01	4.38E-01
    3.98E+09	5.69E-01	1.30E+02	-3.63E-01	4.39E-01
    3.99E+09	5.68E-01	1.29E+02	-3.59E-01	4.40E-01
    4.00E+09	5.68E-01	1.29E+02	-3.56E-01	4.43E-01
    4.01E+09	5.69E-01	1.28E+02	-3.52E-01	4.47E-01
    4.02E+09	5.70E-01	1.28E+02	-3.48E-01	4.51E-01
    4.03E+09	5.71E-01	1.27E+02	-3.45E-01	4.56E-01
    4.04E+09	5.74E-01	1.26E+02	-3.41E-01	4.61E-01
    4.05E+09	5.76E-01	1.26E+02	-3.37E-01	4.67E-01
    4.06E+09	5.77E-01	1.25E+02	-3.31E-01	4.73E-01
    4.07E+09	5.79E-01	1.24E+02	-3.25E-01	4.79E-01
    4.08E+09	5.80E-01	1.23E+02	-3.19E-01	4.84E-01
    4.09E+09	5.79E-01	1.23E+02	-3.13E-01	4.87E-01
    4.10E+09	5.77E-01	1.22E+02	-3.07E-01	4.88E-01
    4.11E+09	5.75E-01	1.22E+02	-3.01E-01	4.89E-01
    4.12E+09	5.72E-01	1.21E+02	-2.96E-01	4.90E-01
    4.13E+09	5.70E-01	1.21E+02	-2.92E-01	4.89E-01
    4.14E+09	5.67E-01	1.20E+02	-2.87E-01	4.89E-01
    4.15E+09	5.65E-01	1.20E+02	-2.83E-01	4.89E-01
    4.16E+09	5.63E-01	1.20E+02	-2.79E-01	4.89E-01
    4.17E+09	5.61E-01	1.19E+02	-2.74E-01	4.89E-01
    4.18E+09	5.60E-01	1.19E+02	-2.70E-01	4.90E-01
    4.19E+09	5.59E-01	1.18E+02	-2.65E-01	4.92E-01
    4.20E+09	5.58E-01	1.18E+02	-2.61E-01	4.93E-01
    4.21E+09	5.57E-01	1.17E+02	-2.57E-01	4.94E-01
    4.22E+09	5.57E-01	1.17E+02	-2.53E-01	4.96E-01
    4.23E+09	5.57E-01	1.17E+02	-2.49E-01	4.98E-01
    4.24E+09	5.57E-01	1.16E+02	-2.46E-01	5.00E-01
    4.25E+09	5.58E-01	1.16E+02	-2.44E-01	5.02E-01
    4.26E+09	5.58E-01	1.16E+02	-2.42E-01	5.03E-01
    4.27E+09	5.59E-01	1.15E+02	-2.39E-01	5.05E-01
    4.28E+09	5.59E-01	1.15E+02	-2.37E-01	5.06E-01
    4.29E+09	5.60E-01	1.15E+02	-2.35E-01	5.08E-01
    4.30E+09	5.59E-01	1.15E+02	-2.32E-01	5.09E-01
    4.31E+09	5.58E-01	1.14E+02	-2.29E-01	5.09E-01
    4.32E+09	5.57E-01	1.14E+02	-2.26E-01	5.10E-01
    4.33E+09	5.56E-01	1.14E+02	-2.22E-01	5.10E-01
    4.34E+09	5.55E-01	1.13E+02	-2.19E-01	5.10E-01
    4.35E+09	5.54E-01	1.13E+02	-2.15E-01	5.11E-01
    4.36E+09	5.53E-01	1.12E+02	-2.12E-01	5.11E-01
    4.37E+09	5.53E-01	1.12E+02	-2.07E-01	5.12E-01
    4.38E+09	5.52E-01	1.12E+02	-2.03E-01	5.14E-01
    4.39E+09	5.52E-01	1.11E+02	-2.00E-01	5.15E-01
    4.40E+09	5.52E-01	1.11E+02	-1.97E-01	5.16E-01
    4.41E+09	5.52E-01	1.11E+02	-1.93E-01	5.16E-01
    4.42E+09	5.51E-01	1.10E+02	-1.91E-01	5.17E-01
    4.43E+09	5.51E-01	1.10E+02	-1.88E-01	5.18E-01
    4.44E+09	5.51E-01	1.10E+02	-1.85E-01	5.19E-01
    4.45E+09	5.50E-01	1.09E+02	-1.84E-01	5.19E-01
    4.46E+09	5.50E-01	1.09E+02	-1.82E-01	5.19E-01
    4.47E+09	5.49E-01	1.09E+02	-1.80E-01	5.19E-01
    4.48E+09	5.48E-01	1.09E+02	-1.78E-01	5.18E-01
    4.49E+09	5.47E-01	1.09E+02	-1.76E-01	5.18E-01
    4.50E+09	5.46E-01	1.09E+02	-1.74E-01	5.17E-01
    4.51E+09	5.45E-01	1.08E+02	-1.71E-01	5.17E-01
    4.52E+09	5.43E-01	1.08E+02	-1.68E-01	5.17E-01
    4.53E+09	5.42E-01	1.08E+02	-1.66E-01	5.17E-01
    4.54E+09	5.42E-01	1.07E+02	-1.63E-01	5.17E-01
    4.55E+09	5.42E-01	1.07E+02	-1.60E-01	5.18E-01
    4.56E+09	5.41E-01	1.07E+02	-1.57E-01	5.18E-01
    4.57E+09	5.41E-01	1.07E+02	-1.54E-01	5.19E-01
    4.58E+09	5.41E-01	1.06E+02	-1.51E-01	5.19E-01
    4.59E+09	5.40E-01	1.06E+02	-1.48E-01	5.20E-01
    4.60E+09	5.40E-01	1.06E+02	-1.46E-01	5.20E-01
    4.61E+09	5.40E-01	1.06E+02	-1.44E-01	5.20E-01
    4.62E+09	5.39E-01	1.05E+02	-1.43E-01	5.20E-01
    4.63E+09	5.39E-01	1.05E+02	-1.41E-01	5.20E-01
    4.64E+09	5.38E-01	1.05E+02	-1.40E-01	5.19E-01
    4.65E+09	5.37E-01	1.05E+02	-1.38E-01	5.19E-01
    4.66E+09	5.36E-01	1.05E+02	-1.36E-01	5.18E-01
    4.67E+09	5.35E-01	1.05E+02	-1.34E-01	5.18E-01
    4.68E+09	5.34E-01	1.04E+02	-1.32E-01	5.17E-01
    4.69E+09	5.33E-01	1.04E+02	-1.29E-01	5.17E-01
    4.70E+09	5.32E-01	1.04E+02	-1.26E-01	5.17E-01
    4.71E+09	5.32E-01	1.03E+02	-1.24E-01	5.17E-01
    4.72E+09	5.31E-01	1.03E+02	-1.21E-01	5.17E-01
    4.73E+09	5.30E-01	1.03E+02	-1.18E-01	5.17E-01
    4.74E+09	5.29E-01	1.02E+02	-1.15E-01	5.17E-01
    4.75E+09	5.29E-01	1.02E+02	-1.12E-01	5.17E-01
    4.76E+09	5.28E-01	1.02E+02	-1.10E-01	5.17E-01
    4.77E+09	5.28E-01	1.02E+02	-1.07E-01	5.17E-01
    4.78E+09	5.28E-01	1.02E+02	-1.05E-01	5.17E-01
    4.79E+09	5.27E-01	1.01E+02	-1.04E-01	5.17E-01
    4.80E+09	5.27E-01	1.01E+02	-1.02E-01	5.17E-01
    4.81E+09	5.26E-01	1.01E+02	-1.00E-01	5.17E-01
    4.82E+09	5.26E-01	1.01E+02	-9.80E-02	5.16E-01
    4.83E+09	5.25E-01	1.01E+02	-9.59E-02	5.16E-01
    4.84E+09	5.24E-01	1.00E+02	-9.34E-02	5.16E-01
    4.85E+09	5.23E-01	1.00E+02	-9.07E-02	5.15E-01
    4.86E+09	5.22E-01	9.97E+01	-8.80E-02	5.14E-01
    4.87E+09	5.21E-01	9.94E+01	-8.48E-02	5.14E-01
    4.88E+09	5.20E-01	9.90E+01	-8.14E-02	5.14E-01
    4.89E+09	5.19E-01	9.86E+01	-7.80E-02	5.13E-01
    4.90E+09	5.18E-01	9.83E+01	-7.51E-02	5.13E-01
    4.91E+09	5.18E-01	9.80E+01	-7.23E-02	5.13E-01
    4.92E+09	5.18E-01	9.77E+01	-6.94E-02	5.13E-01
    4.93E+09	5.17E-01	9.74E+01	-6.67E-02	5.13E-01
    4.94E+09	5.17E-01	9.71E+01	-6.39E-02	5.13E-01
    4.95E+09	5.16E-01	9.68E+01	-6.11E-02	5.13E-01
    4.96E+09	5.15E-01	9.66E+01	-5.89E-02	5.12E-01
    4.97E+09	5.14E-01	9.63E+01	-5.68E-02	5.11E-01
    4.98E+09	5.13E-01	9.61E+01	-5.47E-02	5.10E-01
    4.99E+09	5.12E-01	9.59E+01	-5.25E-02	5.09E-01
    5.00E+09	5.10E-01	9.56E+01	-5.02E-02	5.07E-01
    

    Regards,

    Vijay

  • Hi

    Thank you.

    I will look into this. As the S parameters are in differential mode, is my understanding correct that impedance transformers are not required.

  • Hi Maxplus,

    You are correct. Impedance transformation is not required.

    Regards,

    Vijay