Dears,
About the ADS1281,The datasheet does not show the ESD rating of the device, and the wet sensitive MSD rating, how about the parameter. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hui,
I was able to lookup the ESD ratings for the ADS1281IPW...
For HBM the device is rated up to 2 kV.
For CDM the device is rated up to 500 V.