Part Number: ADS1120
Other Parts Discussed in Thread: ADS1231, ADS124S08, ISOW7842
Hi experts,
I have a question regarding the ADS1120’s internal low-side switch, for bridge sensors:
If I have the ADS1120 connected to a bridge sensor, and a sensor fault occurs that shorts out the bridge sensor, is there a specification for how long the low-side power switch can tolerate sinking that short-circuit current (in my case, ~130mA) before my system is able to switch it off? I know it is specified for 30mA steady state, but I don’t see an absolute maximum rating for it, or something I can use to guess at how fast it could heat up and damage the device.
Thanks,
Reed