Hello,
I'm working on debugging a spur which is located right in the center of the passband(At the typical location of the interleaving spur).
This is strange as we are running only one channel of the ADC in non-DES mode.
This spur is quite high(~ 20dB above the noise floor), and the level will vary from power up to power up.
We are running the ADC at 1600MHz, using only the Q Channel. Our RF signal is then centered at 1200 MHz.
I do not see any spurs at 1200 MHz when I probe the input pins, so I believe this is generated inside the ADC.
Any ideas where this could be coming from?
Thank You,
Will