This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45EVM: Register settings for bypass mode and DDC usage

Part Number: ADC32RF45EVM


Hello,

I am trying to setup ADCRF45 device in bypass mode. I am going through the instructions in user manual. In figure 4 of section 3.2, you show the DDC configurations. Why do we need to setup DDC. I thought DDC is bypassed in this case.

Can you please clarify?

If it is required, what those numbers really mean? 

Thank you.

Mallesh

  • Hi Mallesh,

    Wrong GUI snapshot is used as figure 4 in section 3.2 by mistake. However the instructions in the section are correct. 

    The correct snapshot is below. Please use this as reference to configure the ADC in bypass mode. 

    Regards,

    Vijay

  • Thank you Vijay for your quick reply.

    I have another question regarding register writes.

    Register writes recorded by evm programming are as follows. 

    Write Register: ADC32RFxx_DIGITAL.JESD DIG CHB 0x02 0x690002 0xF
    Write Register: ADC32RFxx_DIGITAL.JESD DIG CHA 0x02 0x1690002 0xF

    For this example writes, 

    In my own driver, 

    Do I need to write the following,

    0x4001     0x00

    0x4002     0x00

    0x4003     0x00

    0x4004     0x69

    0x6002     0xF              // write for channel A

    0x7002    0xF               // write for channel B

    Is this correct? THis applies only to JESD page.

    For all other digital pages, I need to change 0x4003 to 0x1 for selecting channel B. Is that correct?

    Please let me know.

    Thanks,

    Mallesh

  • Hi Mallesh,

    Sorry for the delay. I missed this post as it was marked as 'resolved'. 

    Your understanding of digital page selection is correct. The same is explained in section 8.4.3.3 of datasheet for your reference. 

    Configuration files for ADC32Rfxx devices are also available at this link: www.ti.com/.../SBAA226

    Regards,

    Vijay