Hello to forum members and Texas Instruments staff.
I want to use the ADS4245 in application where my sampling frequency is 36 Mhz and my signal is baseband, 30 Mhz bandwidth. (I am sampling "I" and "Q" signals and reconstructing them digitally, hence the under-Nyquist sampling frequency).
I need to have 50 ohm, isolated input, and want to have voltage gain in my input stage - using 1:4 voltage transformer, so I will have 1:16 impedance transform, and for 50 ohm input I need to terminate the ADC with ~800 ohm "source resistance".
The datasheet says that by using the "high source resistance' the circuit will suffer from inability to smooth out glitches caused by sample-and-hold capacitor switching inside the ADC chip, and I will have "degraded performance".
Quote from the datasheet: "The higher source impedance is unable to absorb the sampling glitches effectively and can lead to degradation in performance (compared to using 1:1 transformers)."
My question is - is this relevant for my relatively low sampling frequency? Maybe it's even more relevant since my the sample-and-hold switching frequency is close to my signal bandwidth?
Best regards,
Oleg.