Part Number: ADS114S08
Hello,
For unknown reason when I try to read Temperature over SPI ADS114S08 just return 0's. While there is no problem to read any of the external analog inputs. All registers reads and writes ok.Means SPI communication is ok. Device is set in single conversion mode, conversion is started with START pin, then waiting for DRDY low, which occurs in expected time - just same as it does with external AINx connected. Means conversion happens. Also tried to measure power rails by changing SYS reg value - also no luck. I suspect something wrong with internal interconnect?
Can somebody confirm that Temperature is realy readble on real part? Or anything wrong in my circuit? Or something wrong with registers? Here is attached connections and also registers dumped from real life part right after the end of conversion.