Part Number: AMC7834
Hi there,
have several AMCs on my board and already using them as expected. But one of them is working differently and not sure if it is damaged or what I can do.
Normally when the AMC is clamping it goes with the DAC bipolar to -5V. But at one AMC (only one of that DAC pairs) is Always going to around 0V instead. So AVss -5V is working properly cause the 2nd bipolar DAC seems to work and clamping.
The DAC itself is also working when I write the Register...I can set around -5...0V manually via SPI. So it seems it is electrically capable. But only when it gets a clamping command...it`s not.
Thanks and regards,
Markus