This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8318: Provide the alloy used for lead finish of this component.

Part Number: ADS8318

Hi

as per one of the PCN#20191010001.1, lead finish is getting changed from NiPdAu to Matte Tin.

One of the part being used by us is affected bt this notice.

Part number : ADS8318IBDGST

1) Please let us know wheather,Nickel-layer used under matte tin is an option or can be one in the future

2) Please specify the thickness of matte tin plating information.

 

Thanks & Regards,

Sandesh Naik

20191010001.1