Part Number: ADS1294R
Hello,
I want to set the common mode without using RLD Electrode.
Our ADS1294R is confiigured for only 2 electrodes.
In the datasheet, Figure 95 shows how to connect RLDINV and RLDOUT to the input through pull up resistor.
- Do you know pull up resistor value? (Is 10M Ohms too high)?
- what about the RLDREF and RLDIN connection? Do I have to keep them not connected or do I have to connect them somewhere?
Thanks
Damien