Hello everyone,
We had some noise on the DAC outputs of DAC60508.
We are using this chip with compatible QFN to dip adapter. The CS pin of the chip is pulled up with 10k resistor. Also, a 100pf capacitor is added between CS and ground. The SPI master (STM Nucleo F746zg) sends 0xCCC0 (approximately 4V) to the DAC2 register. The yellow signal is representing the DAC2 output in the figure. But there is noise on the DAC2 output when the SPI clock (green signal) active. According to the Figure 48 on the datasheet these noise is approximately 1mV.
Could you have any explanation why the noise level is too high?
The chip configuration registers are settled as follow:
SYNC : 0x0000
CONFIG : 0x0000
GAIN : 0x00FF