Part Number: DAC8775
Hello team,
I'm using the DAC8775 in some new boards.
The value is still within the stated tolerance specification, but I was intrigued that the graphs on p. 29 of the DS report Vref values around 4.995V, i.e. 'low' of -0.1%.
It therefore seems that 4.995V, instead of 5.000V, is the most probable value for the Vref of the DAC8775.
Is there a graph of the distribution of the value of the Vref?
Also I noticed that the chip has registers to calibrate gain / offset.
Gain values> 1.000 can be set. But this does not allow me to increase the full scale voltage anyway, so I don't understand its usefulness.
Ultimately, it seems to me that the only solution to reach 10.00V with internal Vref is to use the 12.00V range.
It's correct ?