Part Number: DAC8750
Hello everybody !
I'm writing here because I have a problem on the DAC8750.
In my PCB, I have two DAC8750 in daisy chain mode and I followed your instructions regarding the protections while designing the circuit.
Firstly, I tried to supply the AVDD with 24 V, letting one of the two chip generate the DVDD (pulling its DVDD-EN pin high) for the rest of the circuit (in particular for the other DAC and for the two optoisolator).
With this configuration, the chip which generated DVDD has often burned out, so I decided to pull its DVDD-EN pin low and generate the DVDD with a voltage regulator (from AVDD).
In this configuration, when I supply AVDD with 12 V, the circuit seems to work fine, but when I supply with 24 V, the DAC burns again.
I attach here my schematics.
Thank for your help !
Leonardo