Hello Alex,
So i replaced the chip , and now the vcap1 volatage is correct, but the 4.5v between VREFP and VREFN is not there, I did check with the ads1299EVM board for our mux settings via our micro-controller board and that works fine. When we read back the mux settings in our ADS1299 pcb , the mux settings are correctly written but the voltage is not generated between VREFP and VREFN.