Other Parts Discussed in Thread: ADS127L01
Hello guys,
One of my cutomers is looking for a ADC device which can start sampling data and conversion after one pulse input.
Their requests spec for the ADC are the follows.
1. 18bit.
2. 500kSPS.
3. INL=+/-1.5dB.
4. 1 channel differential input.
5. SPI IF
6. AD converter that starts sampling and converts after that when one timing signal is input.
Do you have any ADC device which can be suited for the above?
Your reply would be much appreciated.
Best regards,
Kazuya.