Other Parts Discussed in Thread: ADS124S08, ADS1247
Hello
We develloped some year ago some application using ADS1248.
I have 3 questions:
1- Can I replace the ADS1248 by the ADS124S08, without change anything else? (Spi communication, Register access, hardware ..) Just keeping in mind the new one has two channel, then we don't use the 4 last channel..?
2- We devellop one application based on the ADS1248, but using only the AD0 ..AD3 based on the ADS1248 datasheet p76:
Figure 114. Ratiometric 3-Wire RTD Measurement System Featuring the ADS1247
With this, we have one channel of PT100 sensor.
Today, if we want add a channel of PT100, using the AD4..AD7, how can I adapt the schematic relatif to the REFP/REFN?:
- a) Can I have twice Ref filter from pin REFP0/REFN0, then duplicate all the schematic composed by the (CR_CM1, CR_CM2, CR_Diff, Rr1, Rr2)
- b) Keep only one Ref filter (CR_CM1, CR_CM2, CR_Diff, Rr1, Rr2) and have the lead 3 of 2 PT100 common?
3- New application note for the ADS124S08:
https://www.ti.com/lit/an/sbaa334/sbaa334.pdf
"Three-wire PT100 RTD measurement circuit with low-side reference and one IDAC current source".
The schematic is a little different on the "Lead 3" / AIN3.
- Is a specific for the new ADS124S08? Or twice schematic can be applied on both ADS1248 AND ADS124S08?...
- Which is the difference between the two solutions?
Thank