Other Parts Discussed in Thread: ADS1292
I want to use ADS1292 for EMG acquisition. I have to monitor two muscles hence I need to use two channels (1P, 1N and 2P, 2N also a reference electrode). Since ADS1292 is for ECG application, the input pins (ELA, RL, ERA etc) are quite confusing for me. I have the ADS 1292 PDK evaluation board with me. So how do I connect the electrodes to the DB9 connector for EMG input? I figured out tapping points for these input channels across C92 and C91 by avoiding the rest of the circuitry between the IC and DB9 connector (see attachment named input channels). Are those the right places to connect the electrodes? However still I haven't found a location to connect the reference electrode or is the reference electrode mandatory?