Team,
I need a favor. Referring to ABSOLUTE MAXIMUM RATINGS on page 2 of the attached file.
The absolute maximum rating across (differential voltage) AINP & AINN for both AC and DC have a range, instead of a single number.
For example, for AC: 1.25V to 3.75V, if the device will not be damaged with ±3.75V across input stage,what does ±1.25V. refer to aka What is the lower number for in these specs? Same for DC case.
Thank you for your help.