Part Number: ADS1261
Hi,
We plan to use ADS1261 in our design.There are 10 analog single-ended signals with voltage range from 0 to 4.5V. We plan to connect them to AIN0 through AIN9. AVDD will be powered at 5V and also used as reference voltage. After reading the datasheet, I come up a few questions and hopefully you can help me clear them up:
1. Should AINCOM be connected to analog ground? Could it be left floating? Does each of analog input have to use AINCOM as its ground reference?
2. Could we use ADS1261 internal PGA with its gain set to 1 or have to bypass it in our case?
3. Since the internal 2.5V reference voltage is not use, could we leave REFOUT pin open without 10uF capacitor?
4. Are there any other things we have to pay attention?
Thank you!
Yong