Part Number: DAC8551EVM
Other Parts Discussed in Thread: DAC8551
Dear Team,
My customer has one motor driver project that would like to use DAC8551 to generate an adjustable voltage.
There is a PWM signal is sent from the motor driver to MCU, MCU would base on this PWM signal to adjust DAC8551 output voltage.
Now they have some questions about EVM block diagram as below.
1. For above application scenario, do they need to use output buffer module(U2_OP AMP)? Why?
2. Could they tie VrefH to external reference module(U3/U8A) directly?
3. Could they tie Vout(pin4) to the input of other device?
Thank you.
Regards,
Jim